AXIS#.HOME.FEEDRATE

Description

AXIS#.HOME.FEEDRATE is the percentage of the homing speed (AXIS#.HOME.V) used when searching for the feedback’s index. AXIS#.HOME.FEEDRATE is only used in home modes 3, 6 and 10.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

This content is not applicable to KAS.

Type

Read/Write

Units

%

Range

1 to 100

Default Value

50

Data Type

Integer

See Also

AXIS#.HOME.V, AXIS#.HOME.MODE

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Related Topics

1    HomingClosedThe Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position